AXIS#.STOP

Description

This command stops drive motion. In torque and velocity modes, the command value will immediately be set to 0. In position mode, the axis will decelerate to a full stop. If the position command is from a gearing master, the drive will cancel gearing and decelerate to a stop. This command has no effect if the command source is an analog input.

If the command values are coming from a fieldbus master, the stop may be immediately overwritten by a new fieldbus command. Use a controlled stop input or disable command to ensure a stop.

The following table defines the behavior of AXIS#.STOP:

Cmdsource Opmode Subopmode Deceleration ramp defined by:
Service Torque - AXIS#.IL.CMD = 0
Velocity - AXIS#.SM.DEC and AXIS#.SM.DEC 
Position Service motion AXIS#.SM.DEC and AXIS#.SM.DEC 
Motion tasking AXIS#.MT.DEC
Homing AXIS#.HOME.DEC
Fieldbus Torque - Command has no effect.
Velocity
Position
Electronic Gearing Position - AXIS#.GEAR.DECMAX
Analog Torque - Command has no effect.
Velocity
Position

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.STOP

5000h

0dh

Unsigned32

-

-

Write only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5016

1

5016 (0x1398)

AXIS1.STOP

Unsigned8

Read/Write

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.STOP

5016

Unsigned8

Read/Write

-